Other Parts Discussed in Thread: MSP430FE4252
Hi!
I'm using MSP430FE4252 in my project. And I need to connect it to the display via SPI.
At first I configure USART module:
//setup USART0 in SPI mode
LCD_MOSI_SEL |= LCD_MOSI_PIN;
LCD_CLK_SEL |= LCD_CLK_PIN;
UBR00 = 0x02;// set baud divide by two
UBR10 = 0x00;
U0CTL |= SWRST;//Reset
U0ME |= USPIE0;//switch On SPI module
U0CTL |= SYNC + CHAR + MM;//SPI 8 bit Master Mode
U0TCTL |= STC;//3-pin SPI mode
U0TCTL |= SSEL1;//use MCLK
U0CTL &= ~(SWRST);//Rest Done
And send to display comand and data without interrupts:
void WriteCommand(uint8_t ucData)
{
// Store current GIE state
uint16_t gie = __get_SR_register() & GIE;
// Make this operation atomic
__disable_interrupt();
ClearCS();
LCD_CD_PORT &= ~LCD_CD_PIN;
while(! (U0TCTL & TXEPT));
U0TXBUF = ucData;
while(! (U0TCTL & TXEPT) );
// CS High
SetCS();
// Restore original GIE state
__bis_SR_register(gie);
__enable_interrupt();
}
Start Debug (CCS V5.5) via MSP30FET and via Logic Analyzer watch next picture
WAT? Inverse Logic in MOSI signal and additional bits in It (there are 12 bits in CLK signal)..
Pause Debug and looking through registers:
All is good (as I think). SPI mode, in U0TCTL CKPH and CKPL are equals zero..
On some other MCU-s USCI module with ~same config works well..
What I need to do to have normal MOSI signal?
PS: I tried to reset U0MCTL with the same result