I am using MSP-TS430PZ100C target board with MSP-FET debugger and IAR version 6.10.1.
When I try to run an "Flash LED code" example code provided by IAR, in debug mode I get the following error.
Firmware version 30400020
Interface dll version 3.4.0.20
Unknown device : (OpenDevice) , Device=MSP430F6438, PwLength=0x0
Fatal error: Could not find device (or device not supported) Session aborted!
Internal error : (SetEEMSequencer)
Fatal error: Closing debug session Session aborted!
I have checked all the jumper settings, also Vcc is supplied internally correctly (Verified by probing Vcc and pin 11 of the controller)
What could be the possible cause of this error?
The chip used is MSP430F6438 with the following IAR settings:
Device description file used : MSP430F6438.ddf
Debugger: FET debugger with Texas Instrument USB-IF connection