Other Parts Discussed in Thread: MSP430AFE222
trying the example "Multiple Time Bases on a single MSP430 Timer Module", with a MSP430AFE222, I used following code: (Compiler MSPGCC)
#include <msp430afe222.h>
int main(void)
{
WDTCTL = WDTPW + WDTHOLD; // Stop WDT
//Calibrate DCO for 8MHz operation
BCSCTL1 = CALBC1_8MHZ;
DCOCTL = CALDCO_8MHZ;
P2SEL |= BIT0; // P2.0 option select
P2SEL2 |= BIT0; // P2.0 option select
P2DIR |= BIT0; // P2.0 - output
P1SEL |= BIT7+BIT6 ; // P1.7 - P1.6 option select
P1SEL2 |= BIT7+BIT6; // P1.7 - P1.6 option select
P1DIR |= BIT7+BIT6+BIT0; // P1.7 - P1.6 - P1.0 outputs
TACCTL0 = OUTMOD_4 + CCIE; // CCR0 toggle, interrupt enabled
TACCTL1 = OUTMOD_4 + CCIE; // CCR1 toggle, interrupt enabled
TACCTL2 = OUTMOD_4 + CCIE; // CCR2 toggle, interrupt enabled
TACTL = TASSEL_2 + MC_2 + TAIE; // SMCLK, Contmode, int enabled
_BIS_SR(LPM0_bits + GIE); // Enter LPM0 w/ interrupt
return 0;
}
// Timer A0 interrupt service routine
#pragma vector=TIMER0_A0_VECTOR
__interrupt void Timer_A0 (void)
{
if(TACCTL0 & CCI) // If output currently high
{
TACCR0 += 1000;
}
else
{
TACCR0 += 500;
}
}
// Timer A1 Interrupt Vector (TA0IV) handler
#pragma vector=TIMER0_A1_VECTOR
__interrupt void Timer_A1(void)
{
switch( TA0IV )
{
case 2: if(TACCTL1 & CCI) // If output currently high
{
TACCR1 += 700;
}
else
{
TACCR1 += 500;
}
break;
case 4: if(TACCTL2 & CCI) // If output currently high
{
TACCR2 += 900;
}
else
{
TACCR2 += 500;
}
break;
case 10: P1OUT ^= 0x01; // Timer overflow
break;
default: break;
}
}
When I run the code, I get three perfect identical frequencies (just as expected). However, the separation of rising and falling edge (TACCTLx & CCI) to get different pulse widths has no effect. Each Pulse still has the same duty cycle ration of 50%, which would mean that (TACCTLx & CCI) is always ZERO. ???
What am I missing?
Thanks for your help!!