Hi,
i have wired my MSP FET according to the 2 wire JTAG schematic i found here:
http://processors.wiki.ti.com/index.php/JTAG_(MSP430)
without the fuse blown i get the communication fine and can program the device. once i click run>advance>make device secure and click ok to blowing the fuse i can not get communication again.
i do not get any message saying fuse was blown. when i try to connect i get
MSP430: Error connecting to the target: Unknown device
i have also tried with the Lite Fet-pro430 software and using the launchpad i can verify the fuse is ok but not blow the fuse as that is not supported.
when i try to connect with the msp-fet using the lite fet-pro430 software i can not verify the fuse is not blown but using code composer i can communicate so i know it's not blown.
is there a simple check i can do to confirm the fuse is blown?
is previous times of programming i had got a message "could not connect as the fuse is blown" this was solved by relaunching the target configuration.
i was expecting the message to say could not connect because the fuse was blown but instead after i blow the fuse i just get a message:
MSP430: Error connecting to the target: Unknown device
look forward to the help as always!
sincerely,
Steven