Hi all!
I`m designing board based on msp430f5256.
And I have some question about schematics.
1. about split-supply I/O
If I don`t using mcu i/o port supply from DVIO domain.
Can I don`t connect DVIO pin to 1,8 V power supply? or DVIO need 1,8 V power supply always?
2. about VeREF
If I don`t using ADC. How correct connect VeREF+ and VeREF- pins. Or it does not have anywhere to connect?
3. about RESET
If I don`t usind BSL and RST/NMI pin that pool-down by default.
Can I don`t connect RST/NMI and reseting MCU by RSTDVCC?
4. about external XT2
If I use external XT2, how connect XTIN and XTOUT pins? Or XTIN and XTOUT pins does not have anywhere to connect?
5. about consume of MCU
How much msp430f5256 consume if it using the following:
- it work in active mode
- external quartz 20MHz
- four USCI on UART mode
- using 3-4 pio
- using DMA
Thanks!