Hi,
I am looking for a MSP430F67651 pin compatible MSP430 controller with DAC outputs
I need minimum 2 DAC outputs.
Is there a MCU with DAC output in 100 pin version
thanks and regards
subramani
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I am looking for a MSP430F67651 pin compatible MSP430 controller with DAC outputs
I need minimum 2 DAC outputs.
Is there a MCU with DAC output in 100 pin version
thanks and regards
subramani
Why don’t you use the product selector on the TI MSP430 homepage? Pick the 100pin case and all the features the 67651 has (and you need) and then select the DAC. Now scan the remaining devices for pin compatibility.
It’s the same job we had to do to answer your question.
But I wonder why you need a pin-compatible version at all. If you didn’t use the DAC before and do now, you already need a new board design to use the DAC. So you can as well change the MSP pinout. If your question was just about the 100pin package, and not a 1:1 pin compatibility, then, well, there are plenty MSP430F4xx and 6xx in 100pin package.
btw: MSPs have either none or exactly two DAC outputs. I don’t remember any MSP with only one or more than two.
**Attention** This is a public forum