Hello,
I am using an MSP430F47196's SD16 to measure mains voltages. The problem I am having is that if the input goes above or below the maximum range of the SD16 (~+-32768), the resulting ADC values do not clip, but fold over. This could happen because of a short term interference spike and I would like to ignore these overrange readings and clip the results to the maximum or minimum values in software for that time. Is there any way to detect in software that the input has overflowed?
Regards
Chris