This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

12Mhz crystal to MSP430F67651

Other Parts Discussed in Thread: MSP430F67651

Can I connect 12MHz crystal to XIN and XOUT of MSP430F67651 

regards

subbu

  • Apparently, the F67651 only supports low-frequency (32768Hz) crystals.
    Experiments with the G2 devices (with a similar limitation) have revealed that in bypass mode, a HF clock signal from an external oscillator with TTL output can be injected (well, not really low-power then, depending on the used oscilaltor). However, this is outside specs and not guaranteed to work with future silicon revisions.
    But, there have been no reports yet for successful trying this with a 5x/6x device.

    If you try., please come back and tell.

  • Thanks Michael,

    We will try it out and come backonce we get PCBA