Hi everyone. Wasn't sure which forum to post this in, the Development Tools forum doesn't seem to have a place for this.
The MSP430 Flasher claims to be under the BSD License --
"The MSP430 Flasher itself is under BSD license, however the package also includes MSP430.dll and HIL.dll which are under "TI Proprietary""
Which BSD License? There are a few different versions. Also, more importantly, where is the source code? There are no links to it from any of the TI Wiki pages about it.
It also mentions that it's compatible with Linux -- however, it then says it's only compatible with Ubuntu, which is not the only Linux... if the source was easily available, I could just build it myself. Not to mention I could help fix the code and submit bug fixes, etc.
Any info would be much appreciated!