This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

use a crystal oscillator instead of crystal on pin 8 and pin 9 clock source. MSP430F235 Urgent!

Configuration 1:

Change to configuration 2

This is the picture of configuration 2:

Can anyone tell me if I can change the configuration 1 to the configuration 2? Configuration 1 is a crystal with 2 terminal. Configuration 2 is a crystal oscillator of four pins. I directly feed the crystal oscillator 32.768 kHz clock output to Xin  pin. I made change on my board. My board does not work. But I do have clock signal on the pin 8. Who can help me?

**Attention** This is a public forum