This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

clock setting sequence using the High Frequency mode

Genius 5960 points
Other Parts Discussed in Thread: MSP430F435

Hi,

I am using the MSP430F435.

The LFXT1 is used in high-frequency mode,
I am going to MCLK / ACLK both use the LFXT1.
(SMCLK stop planned)

MSP430F435 is but I think it works in the DCO by default,
Is there a recommended setting sequence in order to operate in the high-frequency mode?

Best Regards,

hamada

  • The normal answer for this kind of question would be "use driverlib", but that code supports only the low-frequency mode.

    Try copying the code of the CS_XT1Start() function, but change it to set the XTS bit, and to initialize HFFREQ and DIVA.