Hello.
Temperature range for MSP430AFE223IPWR in datasheet is -55...+125*C. Is it correct? But for another package (MSP430AFE223IPW) it is -40...+85:
Thank You/
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello.
Temperature range for MSP430AFE223IPWR in datasheet is -55...+125*C. Is it correct? But for another package (MSP430AFE223IPW) it is -40...+85:
Thank You/
Hi Andy!
I don't think there are different packages for that device. It is TSSOP24 only, or am I wrong?
There are two temperatures mentioned in the datasheet:
and for operation there is:
Dennis
Thank You, Dennis.
But in "addendum page 1" in datasheet is:
MSP430AFE223IPW ACTIVE TSSOP PW 24 60 Green (RoHS& no Sb/Br)CU NIPDAU Level-1-260C-UNLIM -40 to 85 430AFE223
MSP430AFE223IPWR ACTIVE TSSOP PW 24 2000 Green (RoHS& no Sb/Br)CU NIPDAU Level-1-260C-UNLIM -55 to 125 430AFE223
This is problem...
You mean this table:
You are right! There is one entry that says 125°C. That is strange, maybe a typo? I don't know.
Let's see if Katie Pier can get more information about it.
Dennis
My guess would be that this is not a typo but rather is simply the only package of the part that has been qualified for an extended range on the temperature spec - but I'm going to run this one by our team that owns the datasheet to make sure that's correct. I'll let you know as soon as I have an answer.
-Katie
**Attention** This is a public forum