Hi,
I have msp430G2233, I have a task just not sure where to start. I have a result of (0 to 100) and I wan to send to port 1.3(ADC10CLK, VRef, VEref). So the port 1.3 will receive the sum of pulse resulting 0 to 100. Any answer is much appreciated
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I have msp430G2233, I have a task just not sure where to start. I have a result of (0 to 100) and I wan to send to port 1.3(ADC10CLK, VRef, VEref). So the port 1.3 will receive the sum of pulse resulting 0 to 100. Any answer is much appreciated
Yoke Wee Lau said:... I have a task just not sure where to start...
To count all the pulses, you need to start counting before the first pulse arrives, and you need to stop counting after the last pulse arrives. This is not easy unless you have some idea about what period of time the pulses are arriving.
OCY, can you translate? Sorry Yoke, but I do not understand what you are planning to do.
You want to count pulses? But how is that related to ADC10CLK, Vref and Veref? Or do you just mean the pin P1.3 and the datasheet says that this pin has those functions, as well? When counting pulses you should use a pin that can be routed to a timer module. But P1.3 is cannot.
Please tell a little bit more about your project.
Dennis
Hi Dennis,
Sorry for some misunderstanding here.
I might need change the pin in order to use UART.
Basically the project is about the measuring frequency and got the result from 0 to 100. When device pressed read value, sensor will wake up to read current value and send to the device.
My problem now, how to send the value to the device. 8 bits UART?
Thank you
**Attention** This is a public forum