Hello all,
I am running into trouble, I just received a new PCB of mine, on which I wanted very basically use a MSP430F2203 for communication.
Now murphy strikes, and I dont even get the MSP to beeing programmed. I am a little speechless, cannot find my problem or logic error, so maybe you guys and girls can help me out.
I did copy an old PCB file of mine on which the SBW with an MSP430 already working ( I know that for certain, because it went into production :) ) but on this particular PCB it says unknown device. I doubled checked the 4 signals, 3V3, GND, SBWTDIO, SBWTCK, everything is there, no shorts, I even checked with my logic analyzer, the saleae type, I cannot interpret the waveform, but it all looks nice, clock is there as is some data, still unknown device....
So any help appreciated, I assume something must be wrong with communication then, but I got no clue what it could be, I also got 2 PCB built up , same on both of them...