can I use the eZ430-F2013 as jtag for the MSP-EXP430FG4618 Experimenter Board
how it can be done
which setting is needed
thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
can I use the eZ430-F2013 as jtag for the MSP-EXP430FG4618 Experimenter Board
how it can be done
which setting is needed
thanks
natanel said:can I use the eZ430-F2013 as jtag for the MSP-EXP430FG4618 Experimenter Board
Sorry, natanel, but it will only half-work since the EXP430FG4618 has two processors. the eZ430s only support Spy Bi-Wire JTAG which isn't available on the MSP430FG4618. It can, however, work on the MSP430F2013 if you create a custom cable.
**Attention** This is a public forum