Other Parts Discussed in Thread: MSP-TS430PZ100D, MSP430FR6989, MSP-FET
Hello all,
I am using CCS 6.1 and a MSP-TS430PZ100D target board with a MSP430FR6989 in the clamshell. I have been developing a small application, and using the debugging feature to spy memory and such as I manipulate samples from the ADC. Everything was running flawlessly for a while (maybe 10 or so debugging sessions), when all of the sudden I start getting the following error every time I try to debug the program:
MSP430: Trouble Writing Memory Block at 0x4400 on Page 0 of Length 0xe0: Could not erase device memory
MSP430: File Loader: Verification failed: Target failed to write 0x04400
I had not made any significant changes to the program under development...meaning, all I did was change an "int" variable to an "unsigned int" variable. Since this change could not, IMHO, cause the problem with the IDE, I figured I might as well see if anyone else has had this problem and how it was resolved.