This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Program the MSP430F5418A using USB to UART

Other Parts Discussed in Thread: MSP430F5418A

Hi everyone. I have a question to ask about this topic. I have a USB to UART which pin  consists of:-

i. VCC                (DVCC)

ii. TX                  (P1.1)

iii. RX                 (P1.2)

iv. DTR              (RST/NMI/SBWTDIO)

v. RTS               (TEST/SBWTCK)

vi. GND              (DVSS)

 

I connected to my MSP430F5418A as in the bracket. So, basically I will use UART serial interface in order to program my MSP. I tried to program my MSP by using CCS v6. I selected the family and device type of my MSP and I chose UART as my connection. When I click identify and it there was an error which it can't identify target CPU. How do I fix this so that I can burn and program my MSP? Is it something wrong with my pin connection? The USB uses  PL-2303HX chip. I'm not using any LaunchPads or any development board. I soldered the MCU on the LQFP SMD board.

**Attention** This is a public forum