Hello,
I have an issue displaying the output on the terminal when using EM430F6137RF900 with MSP-FET and HMC5883L sensor. When i run just the I2C code with the same setup I could see the output on the console. But when I include the UART code I cannot see the output on the terminal.
When I use the same UART code and using MSP-EXPCC430RFx Experimenter Kit with the same sensor I am able to get the output on the terminal. See the figure below. I hope someone would be able to help me out.