Ref: MSP430F2232 Rev G. Microprocessor
We have come across an issue.
We have a voltage divider consisting of R1 283Kohm (1W 1%) resistor in series with R2 10Kohm (0.125W 0.1%) resistor.
P2.2 connected to R1-R2 junction. Low side of R2 connected to COM - AVss - DVSS Negative Buss.
With a constant DC Voltage 28.44 is applied +R1 & - R2 – COM – Avss – DVSS:
@ 26.4ºC the voltage across R2 measured 0.976 Vdc.
Increasing the Temperature to the Processor
@ 41ºC the voltage across R2 measured 1.050 Vdc.
Result è 11.4ua/18.2ºC {0.626ua/ºC}
When the processor returns to 26.4ºC, and R2 is 0.976 Vdc
The A/D converter is working properly with correctly digitizing the voltage measured. We think that somehow the P2.2 input is back feeding current into R2.
In the spec sheet on page 12 the PORTS (P1, P2, P3, and P4) leakage current is ± 50nA MAX @ 25ºC.
What is the Temperature coefficient? We’re seeing 0.626ua/ºC. (Roughly 10x times larger than 50na in 1ºC change)
Is there some way that we have setup/configured the P2.2 port to cause this problem? Its dedicated function is to read the voltage of R2.
Thank you in advance,
Lee Gassaway