Hello
We currently have a product with USB interface using MSP430F5510 and it has been working well. Recently Ireceived two back from field and it fails to enumerate as a USB device. On power up the device goes and performs it initialisation ok e.g lights flash, all IO port are okay etc. So I belive nothing has been damaged. On one unit I re-flashed it and all works okay. On the second unit we removed the MSP430F5510 and I want to use the emulator using MSP-FET430UIP emulator to find out if any part of the flash is damaged. How can I do this? any ideas would be welcomed.