Hello,
I have a trouble with USB function of MSP430.
I would like to ask about it.
The phenomenon is :
When connects MSP430 (MSP430F5507) with PC(Windows 7),"no action" was occured on the PC.
The device list on Windows doesn't include MSP430, and no error message was displayed on PC.
I used the USB CDC example of USB Developers package.
I use XT2 clock for USB,and the frequency is 4MHz, and with XT2 Bypass mode.
I checked the waveform of the USB clock on a oscilloscope ,and that was correct.
When the USB cable is connected to the PC,the USB device state on MSP430 USB Api is "ST_ENUM_IN_PROGRESS",
and the state would not changed from it to another one.
Would you please tell me some hints about this issue ?
I would appriciate if someone could reply to my question.
Regards,
Hiroyasu