Hi everybody,
I'm investigating the possibility of saving in FRAM the state of the microcontroller in case of low supply voltage ( < 2.0 V). I don't want to use external hardware or the ADC10 to supervise the supply voltage. I tried to intercept the interrupt generated by the SVS, but without success. I was only able to figure out after a BOR the cause of the restart. I know that on another micro (e.g. MSP430F5510) there's the possibility of managing the SVM thresholds in order to generate an interrupt when the supply voltage is falling. Has anyone ever tried to do something like that on MSP430FR5739?
Thank you in advance,
Davide