I tried to compile the example code, it seems OK, but linking could not generate an executable obj.
Including "cs.h", which has definition of function CS_setDCOCenteredFrequency(...), does not help.
Thank you very much in advance for your help.
Below are the console error messages.
**** Build of configuration Debug for project UART **** "C:\\ti\\ccsv6\\utils\\bin\\gmake" -k all 'Building file: ../uart_pc_echo_12mhz_brclk.c' 'Invoking: MSP432 Compiler' "C:/ti/ccsv6/tools/compiler/ti-cgt-arm_5.2.6/bin/armcl" -mv7M4 --code_state=16 --float_support=FPv4SPD16 --abi=eabi -me --include_path="C:/ti/mspware/MSPWare_2_30_00_49/driverlib/driverlib/MSP432P4xx" --include_path="C:/ti/ccsv6/ccs_base/arm/include" --include_path="C:/ti/ccsv6/tools/compiler/ti-cgt-arm_5.2.6/include" --include_path="C:/ti/ccsv6/ccs_base/arm/include/CMSIS" --advice:power=all -g --gcc --define=__MSP432P401R__ --define=TARGET_IS_MSP432P4XX --define=ccs --diag_warning=225 --display_error_number --diag_wrap=off --preproc_with_compile --preproc_dependency="uart_pc_echo_12mhz_brclk.pp" "../uart_pc_echo_12mhz_brclk.c" 'Finished building: ../uart_pc_echo_12mhz_brclk.c' ' ' 'Building target: UART.out' 'Invoking: MSP432 Linker' "C:/ti/ccsv6/tools/compiler/ti-cgt-arm_5.2.6/bin/armcl" -mv7M4 --code_state=16 --float_support=FPv4SPD16 --abi=eabi -me --advice:power=all -g --gcc --define=__MSP432P401R__ --define=TARGET_IS_MSP432P4XX --define=ccs --diag_warning=225 --display_error_number --diag_wrap=off -z -m"UART.map" --heap_size=1024 --stack_size=512 -i"C:/ti/ccsv6/ccs_base/arm/include" -i"C:/ti/ccsv6/tools/compiler/ti-cgt-arm_5.2.6/lib" -i"C:/ti/ccsv6/tools/compiler/ti-cgt-arm_5.2.6/include" --reread_libs --warn_sections --diag_wrap=off --display_error_number --xml_link_info="UART_linkInfo.xml" --rom_model -o "UART.out" "./msp432_startup_ccs.obj" "./uart_pc_echo_12mhz_brclk.obj" "../msp432p401r.cmd" -l"libc.a" <Linking> remark #10371-D: (ULP 1.1) Detected no uses of low power mode state changing instructions undefined first referenced symbol in file --------- ---------------- CS_setDCOCenteredFrequency ./uart_pc_echo_12mhz_brclk.obj GPIO_setAsPeripheralModuleFunctionInputPin ./uart_pc_echo_12mhz_brclk.obj error #10234-D: unresolved symbols remain error #10010: errors encountered during linking; "UART.out" not built >> Compilation failure gmake: *** [UART.out] Error 1 gmake: Target `all' not remade because of errors. **** Build Finished ****