Hello,
We would like to program a MSP430FR5889 via JTAG interface and an Elprotronic FlashPro430 programmer.
The JTAG communication always fails with this error message: "The target microcontroller type does not match selection. Selected microcontroller type MSP430FR5889. Target microcontroller type: 5249"
If we change the processor type in the Elprotronic FlashPro430 programmer to MSP430F5249, the JTAG communication initialization is ok,
but erasing memory fails at next.
But the target microcontroller is definitly an type MSP430FR5889 (printed code on housing).
The same effect occurs, if we try to program the microcontroller from IAR embedded workbench.
What is wrong with our programming setup?
Thank you for your help in advance.
With kind regards,
Thomas