Hello,
I'm using an MSP430F2131. I want to set the LFXT1Sx for a 1-3Mhz crystal for lower power consumption. The actual crystal is however 4Mhz.
Can anyone tell me what the consequences are of this mismatch, if any?
Thank you in advance,
Michael
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
I'm using an MSP430F2131. I want to set the LFXT1Sx for a 1-3Mhz crystal for lower power consumption. The actual crystal is however 4Mhz.
Can anyone tell me what the consequences are of this mismatch, if any?
Thank you in advance,
Michael
The only consequence (in this case) is, that you don't save as much power as you could.
The main difference in the settings is that higher frequency crystals require a higher power injection by the oscillation driver. For slower crystals this may be reduced. So if you run on the 4MHz setting, you waste some power, but I don't expect any other consequences.
In the opposite case, it is possible that the crystal oscillation will cease or will be not stable or at a wrong frequency because of a too-low driver strength.
If I understand correct, my case is the "opposite case" (i.e. 4Mhz crystal wil low frequency setting). Which if I understand correct would result in a lower power injection than necessary with instabilliy and wrong frequencies as a result.
Thank you for your answer
Yes, you're right.
I undestood your initial question in a way that you're using a 4MHz crystal right now by want to replace it by a slower one (without changing the code). Which would of course save much power. :)
It might work anyway. It completely depends on the crystal and the quality (ESR) of the used capacitors. If you use very-high quality capacitors and a good crystal, the lower settings might work without problems.
But I wouldn't risk it. If you build another device later, you'll probably won't get the same quality components or even forget about that and wonder why it doesn't work.
**Attention** This is a public forum