This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430F2112 USCI number

Other Parts Discussed in Thread: MSP430F2112

Hello,

In the IC description on: www.ti.com/.../msp430f2112

says: 16-bit Ultra-Low-Power Microcontroller, 2kB Flash, 256B RAM, 10 bit ADC, 1 USCI

However at page 15 It can be read:

USCI_A0 provides support for SPI (3 or 4 pin), UART, enhanced UART, and IrDA.

USCI_B0 provides support for SPI (3 or 4 pin) and I2C

Does it have 2 independent modules?

I need simultaniusly I2C and UART. Is it possible with MSP430F2112 ?

Many thanks

BR

**Attention** This is a public forum