This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430F6779 building code with Code Composer instead of IAR Embedded Workbench

Other Parts Discussed in Thread: MSP430F6779, TIDA-00222

Hi All,

I'm evaluating the MSP430F6779 chip to be used for power monitoring. I downloaded the reference design from:

http://www.ti.com/tool/tida-00222#descriptionArea

and had the board fabricated and assembled.  I was then able to compile the source code given on the reference webpage and bring the board up.

Unfortunately the source code is built using IAR Embedded Workbench, but when I try to port it to Code Composer I keep getting Error #10099-D "program will not fit into available memory. run placement with alignment fails for section ".infoD" size 0x90. 

Can someone point me to a Code Composer based project for this design?  (Surely since Code Composer is a TI product along with MSP430 chip a project folder must exist. : )  )

(I've spent hours trying to shrink the size of the code and other optimization type tricks but no luck.)

thanks much for any help,

Bob

**Attention** This is a public forum