This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OTA update for msp430fr6989

Other Parts Discussed in Thread: MSP430FR6989, MSP430FR6889

Hi,

 I have msp430fr6989 and want to perform OTA for the same. The system will work like: firmware is received from a gateway and is saved in external flash (SPI interface). Now the bootloader should copy this image from external flash to internal flash and execute it. How it can be done in msp430fr6889. I have searched the forum and many are suggested to use MSPBoot. However, MSPBoot for msp430fr6989 with 20bit support is not yet released. Also,I am using contiki OS and the released MSPBoot has support for only IAR and CCS platforms. How can I migrate the tools to Eclipse in linux?

Waiting for a reply.

**Attention** This is a public forum