Hello All,
I am working on msp430f67641 mcu.
I am confuse about using the PWM in UP_mode and Capture in Continue_Mode of same channel.
my setup:-
PWM :- P3.3/PM_TA0.2
Capture Mode :- P1.1/PM_TA0.1/VeREF+/A1
i using PWM for the LED brightness control and Capture mode for the audio detection. When running the separate code it is working fine but when i merge it is not working.
My code:-
void mic_init(void)
{
TA0CTL = TASSEL_2 + MC_2 + ID_3; // Timer A 0 with SMCLK @ 8MHz, count UP
TA0CCTL1 |= CM_1 + CCIS_0 + SCS + CAP + CCIE; // Raising Edge + CCI0A + Sync + Capture Mode + Interrupt enable
// MIC pin intialize
P1DIR &= ~(BIT1); // make the pin as input
P1SEL |= (BIT1); //set this bit as Input Capture (TA0.CCI0A)
_BIS_SR(GIE); // Global interrupts enabled
prev_count = TA0R; // save the previous count
}
void rgb_led_pwm(void)
{
// Configure RGB Led Pins As Output and PWM control
P3DIR |= BIT3;
P3SEL |= BIT3;
TA0CCR0 = 5000-1; // PWM Per`iod
TA0CCTL2 = OUTMOD_7; // CCR2 reset/set
TA0CCR2 = 0; // CCR2 PWM duty cycle
TA0CTL = TASSEL_2 | MC_1 | TACLR; // ACLK, up mode, clear TAR
}
I am stuck here..give me the solution...