Hello there:I am using MSP430fe4272 for single phase electric energy measurment,the watch crystal I am using is a surface mounted oscilator of AVX Corp/Kyocera Corp with a 32768 hz oscillating frequency,which requires a 7pf load capacitance.on the hardware external capacitors of 7pf each are added.in some boards my code works fine but on others,only some segments of the LCD are visible and an oscilator fault flag is turned on. The same code results different output
I tried by removing the external load capacitors and configure the internal load capacitors,in this case the oscilator fault flag is reset but the LCD is still not functioning.
I guess that there is a problem on oscilator configuration
any thing I should do please?