I am using MSP430F427A with SD16 ADC for single phase energy meter application.
When I set the SD16 for higher sampling rate (4Mhz) then the sample values gradually decrease even if the input is kept unchanged, and sets down after few minutes to a constant value. But if I decrease the sampling rate (to say 1MHz), the sample values are stable.
I am new to the MSP430 world, please suggest any solution.
Thanks in advance.