This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430AFE SD24

Other Parts Discussed in Thread: MSP430AFE251

Hello


We would like to use MSP430AFE251 in submetering application and we need following information about SD24 and PGA:

SD24:

  • TUE
  • Max INL
  • Max Offset
  • Max gain error
  • CMRR
  • Temperature dependency of all factors  from 0 to 85 C

 

Integrated PGA:

  • Temperature dependency from 0 to 85 C
  • Offset
  • Max gain error

Thank you!

Danijel

  • Hello Danijel,

    All available specifications for the SD24 on the MSP430AFE251 are located within the MSP430AFE251 datasheet, which can be found on its product page ( MSP430AFE251). We have no additional information about specifications outside the datasheet. All datasheet specifications are typically tested at the full range of Recommended Operating Free-air Temperature unless specifically stated otherwise by the datasheet.