When using the bsl-scripter-windows.exe for my MSP430F5507 it terminate!
MODE 5xx USB
Unable to open the HID device
Before that i get windows warning USB unit not recognized
- is that expected error/warning?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
When using the bsl-scripter-windows.exe for my MSP430F5507 it terminate!
MODE 5xx USB
Unable to open the HID device
Before that i get windows warning USB unit not recognized
- is that expected error/warning?
Hello Tobias,
Can you post the error message you are getting?
When you put the device into BSL mode, it should show up in Device Manger as a HID device with VID of 0x2047 and PID of 0x200. If you see the HID device then it is ready for BSL download.
Are you using TI EVM board with the MSP430F5507 or your own custom board?
Regards,
Arthi
Hi Arthi
The error message on PC when connection MSP is "Device not recognized"
I get Device USB\VID_0000&PID_0002\6&2dc4c7c1&0&2 from Device Manager!
Using my custom board the VUSB == always high
PUR is controlled by user bottom
BR Tobias
Hi Tobias,
When a device is placed in BSL mode it should show up in Device Manager as VID = 0x2047 and PID = 0x200. My concern here is that even when you connect your custom board to the PC it gives you a "Device not recognized" message may mean that your hardware layout might not be correct.
Document SLAA457.pdf, figure 8, shows how to start a custom USB design.
Regards,
Arthi
**Attention** This is a public forum