Hi Champs,
Customer was checking TI website for latest info on Captivate technology, and has seen a lot more info is now available. Customer projects requires(with most of time) (very) high noise immunity needs. Customer was wondering if TI already challenged this solution to the edge?
best possible Captivate performance reported in documentation/testreport:
Class A Immunity Table (Fully Functional in Presence of Noise)
Sensing Method |
Sensor Type |
Achievable IEC 61000-4-6(Conducted) Level |
Self |
Buttons |
Level 3 (10V RMS) |
Self |
Sliders/Wheels |
Level 3 (10V RMS) |
Customer questions:
Which maximum level could be achieved above 10Vrms ? Some clients are asking for higher immunity (for example up to 30V rms), but we would like to know what could be achieved and seen as really the maximum possible with captivate technology.
Are there test results available above 10Vrms (on certain evaluation setup, certain devices?)
Thanks in advance, Patrick