Other Parts Discussed in Thread: MSP430F2003,
Hello.
I have three questions
1.Could you tell me following values when configuration is the fastest conversion speed in SD24 and SD16 ?
・conversion speed
・resolution that can be used
・current consumption(if possible)
2.Could you tell me following values when configuration is the highest resolution that can be used in SD24 and SD16 ?
・conversion speed
・resolution that can be used
・current consumption(if possible)
3.Are there devices which can realize 16bit that can be used and 1kSPS in MSP430 ?
If answer is "No",would you tell me resolution value that can be used when SD24 and SD16 is configured at 1kSPS.
Incidentally, I am going to use MSP430F2003 and MSP430I2020.
Regards,
uchida-k