Other Parts Discussed in Thread: ENERGIA, MSP430G2553, MSP430G2231, MSP430G2452
I'm wanting to quickly prototype a product with energia sketches (Energia 18) in CCSv7 working with different MSP430GXXX devices. When I create a sketch it defaults me to the MSP430G2553. I have a bunch of MSP430G2202's that I would like to use instead. When I right click on my project and go to Properties->General->Variant and set it to the MSP430G2202 it creates a new config file and sets it as active for me. Everything compiles fine, but when it trys to load it to the board I get the following error
MSP430: Trouble Writing Memory Block at 0xc000 on Page 0 of Length 0x34a: Could not write device memory
It looks to me like the target board is not actually changing and its still attempting to write to the memory location used for the G2553. So i dug further and under Properties->Build->GNU Compiler->Runtime the target wasnt changed. So i changed to to G2202 and now I'm getting compilation errors...
Are other MCU's other than G2553 supported when using Energia sketches?
If so, what is the process to get them functioning?
Thanks