Greetings,
At startup the MSP430FR5859 runs at 2.1V in active mode - no problem.
After startup, the CPU supply voltage is switched from 2.1V to 1.8V. When the supply voltage ramps down (about 7ms later) to about 1.81V the processor resets before it gets to 1.8V. The CPU will run at 1.82V, but below that I get a reset. Is there a way to disable the low-side SVS for this processor, or should I try to solve the problem a different way?
The problem happens with the MSP FET tool and in stand-alone release mode.