Hello.
I am facing following FLL problem in MSP430F447.
However I'm using FLL, DCO frequency is not stable.
For example, when changing the temperature from 25 ° C to -10 ° C, the DCO clock frequency on which FLL is operating changes by 10%.
(I measured SMCLK signal sourced DCO from clock output port.)
The register settings is as follow.
I'm using DCO with FLL at 655.360MHz.
faclk:32.768kHz(crystal)
SCFQCTL:N=19
SCFI0=0
FLL_CTL0=0xA3
FLL_CTL1=0x20
SCG0 is always 0.
When I changed to N = 31 in SCFQCTL register and set the frequency of the DCO clock to 1048.576 KHz,
The frequency change by changing temperature disappeared.
This problem has occurred in multiple devices, but it does not occur on all devices.
Is there something wrong with my setting or anything that could cause this problem?
Would you mind trying out if this problem is reproduced in TI too?
Regards,
uchida-k