Other Parts Discussed in Thread: MSP430WARE, MSP430F2274, MSP430FR2311
Hi,
I have to sample an ADC at 1 KHz and then do some processing based on the ADC reading.
I have a power supply that can source 400uA max for the 430.
The whole design is to monitor 3 voltage rails, 1 with the ADC, the other two are simply digital on/off. The ADC readings are for a scaled AC, so it will need to reconstruct the 60hz AC waveform based on the 1K Hz signal and estimate the peak. It then sends a "you are drooping - better shutdown" GPIO to the big host processor.
For a G series (G2232), I can use a big cap on the micro to give it some holdup on the 3.3v so the 400uA can be supplemented by the capacitor if I wake, run at full speed, then go into sleep mode.
My question is based on the 1K Hz ADC sampling rate, should I run very slow and stay on all the time (and how slow do I have to run to meet a 400uA steady state worsts case), or run very fast and sleep most of the time waking 1000 times a second to sample the ADC? This question centers around my 400uA max average power for the power supply.
It is a telecom application, so I have to meet worst case spec's for everything.
Best Regards,
Blake