Tool/software: Code Composer Studio
Hello,
I am trying to write code for msp430f6438 in ccs7.1 by driverlib.
I got a problem here.
For example, I want stop WDT by call the function " void WDT_A_hold(uint16_t baseAddress)" of driverlib. The Parameters
baseAddress is the base address of the WDT A module (MSP430F5xx_6xx_DriverLib_Users_Guide.pdf page 492)
In "MSP430F6438.H", There is a define which is " #define __MSP430_BASEADDRESS_WDT_A__ 0x0150"
In "MSP430F6438 datasheet page 32", there is "Table 24. Watchdog Registers (Base Address: 015Ch)"
I am confuse. Is there some one can tell me which one is correct and can put in the "void WDT_A_hold(uint16_t baseAddress)"
Thanks,
Dison