Port 1 bit 7 is used for checking the interrupt.
#include <msp430F2616.h>
#define DR P5OUT = P5OUT | BIT7 // define RS high
#define CWR P5OUT = P5OUT & (~BIT7) // define RS low
#define READ P5OUT = P5OUT | BIT5 // define Read signal R/W = 1 for reading
#define WRITE P5OUT = P5OUT & (~BIT5) // define Write signal R/W = 0 for writing
#define ENABLE_HIGH P5OUT = P5OUT | BIT6 // define Enable high signal
#define ENABLE_LOW P5OUT = P5OUT & (~BIT6) // define Enable Low signal
void check_busy(void);
void data_read(void);
void delay(unsigned int wt);
void init(void);
void init_lcd(void);
void wr_lcd_cw(unsigned char lcd_cmd);
void wr_lcd_dw(unsigned char wr_lcd_dw);
void lcd_msg(unsigned char *ch);
volatile unsigned int a=0,b=0,c=0,d=0,e,f,sec1=2,AS;
//__interrupt void Timer_A (void);
//PIN R/W =
/*
* main.c
*/
void count_increment(void);
unsigned char array[10]={"0123456789"};
int main(void) {
volatile unsigned int i;
WDTCTL = WDTPW | WDTHOLD; // Stop watchdog timer
init();
init_lcd();
delay(1000);
P1OUT &= ~BIT7;
wr_lcd_cw(0x80);
lcd_msg(( unsigned char *)"UP count");
while (1)
{
for(a=0;a<10;a++)
{
wr_lcd_cw(0xC0);
wr_lcd_dw(array[a]);
for(b=0;b<10;b++)
{
wr_lcd_cw(0xC1);
wr_lcd_dw(array[b]);
for(c=0;c<10;c++)
{
wr_lcd_cw(0xc2);
wr_lcd_dw(array[c]);
for(d=0;d<10;d++)
{
wr_lcd_cw(0xc3);
wr_lcd_dw(array[d]);
P1OUT ^= BIT5|BIT6;
delay(1000); // Toggle P1.0 using exclusive-OR
//delay(1000) //while(~(TAIV));1 second delay
}
}
}
}
if(AS)
{
AS=0;
// count_increment();
}
}
}
void count_increment(void)
{
/*if(array[d]<10)
{
d++;
wr_lcd_cw(0xc3);
wr_lcd_dw(array[d]);
}
else if(array[c]<10)
{
c++;
wr_lcd_cw(0xc2);
wr_lcd_dw(array[c]);
}
else if(array[b]<10)
{
b++;
wr_lcd_cw(0xc1);
wr_lcd_dw(array[b]);
}
else if(array[a]<10)
{
a++;
wr_lcd_cw(0xc0);
wr_lcd_dw(array[a]);
}
* }*/
P1OUT ^= BIT7;
sec1 = 2;
}
void delay(unsigned int wt)
{
unsigned int k;
volatile unsigned int i ;
for(k=0;k <= wt ;k++)
{
//for( i = 0 ; i <= 800 ; i++ );
_delay_cycles(16000);
}
}
void lcd_msg(unsigned char *ch)
{
while(*ch !='\0')
{
wr_lcd_dw(*ch);
ch++;
}
}
void wr_lcd_cw(unsigned char lcd_cmd){
check_busy();
P4OUT=lcd_cmd;
CWR;
WRITE;
ENABLE_HIGH;//EN=1
delay(3);
ENABLE_LOW;//EN=0
}
void wr_lcd_dw(unsigned char lcd_data){
check_busy();
P4OUT=lcd_data;
DR;
WRITE;
ENABLE_HIGH;//EN=1
delay(3);
ENABLE_LOW;//EN=0
}
void init_lcd(void)
{
wr_lcd_cw(0x38);delay(10);//LCD in 8 bit mode
wr_lcd_cw(0x0e);delay(10);//LCD in 8 bit mode
wr_lcd_cw(0x06);delay(10);//LCD in 8 bit mode
wr_lcd_cw(0x01);delay(10);//LCD in 8 bit mode
//lcd_content(0x02);//return to home location
}
void init(void)
{
DCOCTL = 0x60;
BCSCTL1 = 0xFF;
BCSCTL2 = 0x00;
BCSCTL3 = 0x20;
IFG1=0X00;
IFG2=0X00;
TACTL = 0x01D0;
TACCTL0 = CCIE; // CCR0 interrupt enabled
TACCR0 = 16000;
P1SEL=0;
P5SEL=0;
P4SEL=0;
P1DIR=0xff;
P4DIR=0xff;
P5DIR=0xff;
//INITIALISE UNUSED PORTS TO SAVE POWER
P2DIR=0XFF;
P3DIR=0XFF;
P6DIR=0XFF;
P7DIR=0XFF;
P8DIR=0XFF;
P2OUT=0X00;
P3OUT=0X00;
P6OUT=0X00;
P7OUT=0X00;
P8OUT=0X00;
P1DIR |= BIT5|BIT6; // Set P4 bits 5 and 6 to output direction
P4DIR = 0XFF; // Set Port 4 as output
P5DIR = 0XFF; // Set Port 5 as output
P4OUT = 0X00;
P5OUT = 0X00;
__bis_SR_register(GIE);
}
void check_busy(void)
{
P4DIR &= ~(BIT7); // make P2.3 as input
data_read();
while((P4IN & BIT7)==1)
{
data_read();
}
P4DIR |= BIT7; // make P2.3 as output
}
void data_read(void)
{
CWR;
READ;
ENABLE_LOW;
delay(2);
ENABLE_HIGH;
}
// Timer B0 interrupt service routine
#pragma vector=TIMERA0_VECTOR
__interrupt void Timer_A (void)
{
sec1--;
//P1OUT^=BIT7;
if(sec1==0)
{
count_increment();
}
AS=1;
//P1OUT ^= BIT5|BIT6|BIT7; // Toggle P1.0
TACCR0 += 16000; // Add Offset to CCR0
//TACTL &= ~TAIFG;
}