Tool/software: Code Composer Studio
Hey,
This question might seem a little childish but hear me out.
Each bit in each PxIN register reflects the value of the input signal at the corresponding I/O pin when the
pin is configured as I/O function. These registers are read only.
• Bit = 0: Input is low
• Bit = 1: Input is high
This is what is given in the datasheet. My question is that if I set one pin as output high then will it show as high for that particular bit in PxIN register.?
Thank you.
Viswanath