Tool/software: Code Composer Studio
Hi There,
I use the MSP-TS430PZ100C (REV1.1) with MSP430F6438 MCU.
I have 2 questions here.
Q1. I want use XT1 with a 32.768KHZ crystal. The resistor R6 and R8 are 0. The crystal come with the MSP-TS430PZ100C board. The C1 and C2 do not soldering anything. But the xt1 did not work.
When I change the UCSCTL6 --- XCAP from 0-3, the xt1 still did not work. I also change c1,c2 to 6pf,9pf and XCAP be changed too. xt1 still did not works. Is there some one know the answer.
Q2. Because the xt1 did not works, the internal oscillator be used automatically. I setup the ACLK output to P1.0 and SMCLK output to P3.4 for measure these clock signal by Oscilloscope.
The ACLK's source is xt1, The MCLK and SMCLK's source is DCOCLKDIV.
When I want setup the DCO for SMLK =10MHz, (UCSCTL1--DCORSEL=4; UCSCTL2---FLLD=4;UCSCTL2---FLLN=609; UCSCTL3----FLLREFDIV=2; rest register keep default value), I get a 9.74Mhz.
When I increate the FLLN, the SMCLK do not change. Is there some one know the reason and explain how to setup the DCO and what mean of the DCO Frequency table in datasheet page 55. Because I think the DCOx and MODx will be adjust by DCO for stabilize a frequency I want.
(Notes: When I setup those register like UCSCTL1--DCORSEL=4; UCSCTL2---FLLD=16;UCSCTL2---FLLN=461; UCSCTL3----FLLREFDIV=12, The SMCL is 1.22MHz, The result is almost correct which mean DCOCLK= D* DCOCLKDIV =16* 1.22MHz = 19.52Mhz; By count form the DCOCLK should be 19.966634667MHz )
Thanks,
Dison.