Hello.
I have 3 questions about the content of the datasheet In page of 37, 38.
1.Does the indicated graph show the total value of current that can be output at all pins on the microcomputer?
2.Is there data when Vcc is 3.6 V?
3.If the answer of question 2 is "No", in page of 37, from Figure 5-5, can I assume that only the current close to 0 mA can flow only when the high output is 3 V?
Regards,
uchida-k