Other Parts Discussed in Thread: ISO1050
Dear all,
I use a MSP430 for a low power application. The board should include a CAN-interface. Therefore I use a SPI/CAN module. Now I have found the Application Report SLLA298 (http://focus.ti.com/general/docs/litabsmultiplefilelist.tsp?literatureNumber=slla298b) from TI and I am a little confused, because on figure 2 there is a connection from RxD, TxD to the ISO1050, without using a SPI/CAN module. Thus I have searched on the TI homepage for a CAN library for the platform MSP430, but I have found nothing regarding MSP430 and CAN. How is the CAN protocol implemented in this application (SLLA298)?
Does anybody use an MSP430 with a CAN interface? How looks like the CAN design with the MSP430 and are there any C-libraries?
Thanks for your help!
Gerd