Part Number: MSP432WARE
Other Parts Discussed in Thread: MSP430WARE,
Hi ,
Last year when I started working with the msp432 Launchpad , I used CCSv6.1.1, and example projects for msp432 were present in MSP430WARE itself.
Due to some reason I had to uninstall CCS and again when I reinstalled same version of CCS, I was not able to find the example projects for msp432 in MSP430WARE.
I searched and downloaded MSP432WARE which had example projects but when I load the project (say the simplest project , LED blink), it is throwing me more than 60 errors.
Even projects in Simplelink_msp432_sdk are not working.
I would not like to upgrade CCS to Version7 since I have many running projects using present version(6.1.1)
I have downloaded three packages: MSP430WARE , MSP432WARE, & Simplelink_msp432_sdk
//******************************************************************************
// MSP432P401 Demo - Software Toggle P1.0
//
// Description: Toggle P1.0 by xor'ing P1.0 inside of a software loop.
// ACLK = 32.768kHz, MCLK = SMCLK = default DCO~1MHz
//
// MSP432P401x
// -----------------
// /|\| |
// | | |
// --|RST |
// | |
// | P1.0|-->LED
//
// William Goh
// Texas Instruments Inc.
// June 2016 (updated) | November 2013 (created)
// Built with CCSv6.1, IAR, Keil, GCC
//******************************************************************************
#include "msp.h"
#include <stdint.h>
int main(void) {
volatile uint32_t i;
WDT_A->CTL = WDT_A_CTL_PW | // Stop WDT
WDT_A_CTL_HOLD;
P1->DIR |= BIT0; // P1.0 set as output
while (1) // continuous loop
{
P1->OUT ^= BIT0; // Blink P1.0 LED
for (i = 20000; i > 0; i--); // Delay
}
}
The above shows the LED pin toggle program.
The text marked in red , I do not understand the different syntax used . it gives errors along with the others in different files
Would be great if somehow could help me out with the same.
Regards,
Maisie