This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430FR5994: SPI configuration of BOOSTXL-DRV8305EVM utilizing MSP430 8-bit mode

Part Number: MSP430FR5994
Other Parts Discussed in Thread: TIDA-00645, DRV8305, MSP430G2553, TIDA-00771, MSP-EXP430FR5994, BOOSTXL-DRV8305EVM

Hi all,

I know about SPI interface, I know about 1-bit communication between SPI modules, but I have trouble to have consistency in communication between DRV8305N and MSP430FR5994 in 8-bit mode even I close each 16-bit packet with nCS. However, there are no issues when connecting DRV8305N with C2000 in 16-bit mode. And I had no issues with other 16-bit mode SPI devices. 

So, I'm confused. :) Can anyone confirm that DRV8305N can communicate with MSP430 through SPI interface without issues?

Alexey

**Attention** This is a public forum