I'm using the SD24 internal voltage reference and a GAIN adjustment of 2. At the table 5-19 there is the VSD24REF described with TYP: 1.158V.
At note (2) from table 5-21 is the full- scale range defind as follows:VFSR+ = +VREF/GAIN and VFSR- = -VREF/GAIN;
The range with my adjustment is: -0,579 .. +0,579V
My question: which analog value are equal to 8000hex and 7FFFhex?
I'm a little bit confused because the differential input range for specified performance ist described as +- 464mV