Other Parts Discussed in Thread: MSPBSL, MSP-FET
Hi,
JTAG seems to be invalidated, so I want to do Chip Erase with BSL, but the following log is output.
(Because I don't have the program file and the predecessor has retired, there is no way to know what the BSL setting is.)
Here is my BSL-Scripter script:
LOG
MODE 6xx UART 9600 COM9
VERBOSE
RX_PASSWORD .\pass32_wrong.txt
RX_PASSWORD .\pass32_default.txt
MASS_ERASE
And here is my output from BSL-Scripter:
---------------------------------------------------------
BSL Scripter 3.3.0
PC software for BSL programming
2017-Dec-04 11:41:21
---------------------------------------------------------
Input file script is : C:/MSPBSL_Scripter_win/bsl-scripter-windows/script_6xx_uart.txt
MODE 6xx UART 9600 COM9
VERBOSE
Verbose mode is now on!
RX_PASSWORD .\pass32_wrong.txt
Read Txt File : C:\MSPBSL_Scripter_win\bsl-scripter-windows\pass32_wrong.txt
[80] [21] [00] [11] [ff] [ff] [ff] [ff] [ff] [ff] [ff] [ff] [ff] [ff] [ff] [ff]
[ff] [ff] [ff] [ff] [ff] [ff] [ff] [ff] [ff] [ff] [ff] [ff] [ff] [ff] [ff] [ff]
[ff] [ff] [00] [00] [91] [fb]
[ACK_ERROR_MESSAGE]Unknown ACK value!
RX_PASSWORD .\pass32_default.txt
Read Txt File : C:\MSPBSL_Scripter_win\bsl-scripter-windows\pass32_default.txt
[80] [21] [00] [11] [ff] [ff] [ff] [ff] [ff] [ff] [ff] [ff] [ff] [ff] [ff] [ff]
[ff] [ff] [ff] [ff] [ff] [ff] [ff] [ff] [ff] [ff] [ff] [ff] [ff] [ff] [ff] [ff]
[ff] [ff] [ff] [ff] [9e] [e6]
[ACK_ERROR_MESSAGE]Unknown ACK value!
MASS_ERASE
[80] [01] [00] [15] [64] [a3]
[ACK_ERROR_MESSAGE]Unknown ACK value!
And here is other output from BSL-Scripter another version:
---------------------------------------------------------
BSL Scripter 3.1.0.0
PC software for BSL programming
2017-Dec-04 11:48:40
---------------------------------------------------------
Input file script is : C:/BSL_Scripter_Windows/bsl-scripter-windows/script_6xx_uart.txt
MODE 6xx UART 9600 COM9
VERBOSE
RX_PASSWORD pass32_wrong.txt
Read Txt File : C:/BSL_Scripter_Windows/bsl-scripter-windows/pass32_wrong.txt
[11] [ff] [ff] [ff] [ff] [ff] [ff] [ff] [ff] [ff] [ff] [ff] [ff] [ff] [ff] [ff]
[ff] [ff] [ff] [ff] [ff] [ff] [ff] [ff] [ff] [ff] [ff] [ff] [ff] [ff] [ff] [00]
[00]
RX_PASSWORD pass32_default.txt
Read Txt File : C:/BSL_Scripter_Windows/bsl-scripter-windows/pass32_default.txt
[11] [ff] [ff] [ff] [ff] [ff] [ff] [ff] [ff] [ff] [ff] [ff] [ff] [ff] [ff] [ff]
[ff] [ff] [ff] [ff] [ff] [ff] [ff] [ff] [ff] [ff] [ff] [ff] [ff] [ff] [ff] [ff]
[ff]
MASS_ERASE
[15]
--------------
If BSL is disabled, is this output correct?
Thank you.