Hi,
On page 2 of Current-Transformer Phase-Shift Compensation and Calibration Application Report - SLAA122 (February 2001), Figure 1 shows mains voltage V, mains current I(in) and the output current I(out).
I(out) is the current that we measure after Current Transformer (CT).
According to the Figure 1, it seems like I(out) leads I(in) by φ.
And the following paragraph confirms that.
Also in the next page, in Chapter 2.2, first paragraph confirms that too by saying "To overcome the problem of phase shift across the CT, the output current could be delayed by the same amount as the inherent phase shift so that both the actual and measured power factors were equal..."
What I think is there is somethink wrong here.
As I know, CT lags the current.
So the graph in Figure 1 should be like I(out) lags I(in) by φ.
And the paragraph in Chapher 2.2 should be like "To overcome the problem of phase shift across the CT, the output voltage could be delayed by the same amount as the inherent phase shift ..."
Am I right?
Thank You.